What are you looking for?

This is Search input need to add more information.

Accurate Water Pressure Measurement

Sensors enable companies to determine a leak or break in the line. Your systems can detect a pressure drop indicating a main line break. As the pressure is being measured and determines significant drop, it will also help locate the closest location for shutoff causing less leakage.

Monitor and meter the amount of water that is being used by using differential pressure sensors to measure the pressure drop across a restriction in the flow. Honeywell also has sensors to measure line pressure, and magnetic sensors that can measure the movement in mechanical flow meters.

Associated Products

Other Applications

Language

Social Media

Site Information

Do Not Sell My Personal Information

Sitemap

Terms & Conditions

Global Unsubscribe

Copyright © 2021 Honeywell International Inc.


Fatal error: Access to undeclared static property: PrismLoader::$aAutoloaders in /var2/www/html/honeywell/prism_library/PrismLoader.inc.php on line 87